Active Rule
The active rule view displays the rule that is active at the slide rule position.
NOTE: The active rule view can be launched from the main toolbar.
The active rule view can also be launched from the main toolbar. It will change to display the active rule at the slide rule position on the model output graph. The slide rule position can be change manually or will change automatically when in playback mode. In this mode, the rule will update automatically as the data progresses past the slide rule.
The display format of the rule outcomes can be modified by the toolbar buttons. A single outcome for only the most probable class or multiple outcomes for each of the classes can be displayed. Each outcome displays the percentage and number of cases identified being of the particular class.
Related topics: